Thermocouple Cables
Thermocouple cable is required to make the connection between the thermocouple and the measuring instrument. The construction is totally similar to the Instrument cables a part the material of the conductors. Thermocouple Extension cables use the same alloys as the thermocouple. Compensating cables use different alloys which have a matched emf output over the appropriate temperature range. The Extension cables are more accurate but more expensive than Compensating.
Here below different constructions of thermocouple cables, to see our full capabilities please download our general catalogue
For more detailed information on the most common available constructions click here